FreeBodyResultsBuilderLocationMethod Enumeration¶
NXOpen.CAE.FreeBodyResultsBuilder.LocationMethod is an alias for NXOpen.CAE.FreeBodyResultsBuilderLocationMethod
-
class
NXOpen.CAE.
FreeBodyResultsBuilderLocationMethod
¶ Bases:
object
Location definition method
Enum Members
Enum Member Enum Member Description Id location is defined by node id Coords location is defined by coordinates Csysorigin location is defined by coordinate system origin -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-