FluidDomainBuilderOutputOptionsType Enumeration¶
NXOpen.CAE.FluidDomainBuilder.OutputOptionsType is an alias for NXOpen.CAE.FluidDomainBuilderOutputOptionsType
-
class
NXOpen.CAE.
FluidDomainBuilderOutputOptionsType
¶ Bases:
object
Represents the output types.
Enum Members
Enum Member Enum Member Description BodyOnly The output type specified as only body generation. BodyandMesh The output type specified as body and mesh generation. MeshOnly The output type specified as only mesh genberation. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-