FluidDomainBuilderIntExtType Enumeration¶
NXOpen.CAE.FluidDomainBuilder.IntExtType is an alias for NXOpen.CAE.FluidDomainBuilderIntExtType
-
class
NXOpen.CAE.
FluidDomainBuilderIntExtType
¶ Bases:
object
Represents the interior/exterior types.
Enum Members
Enum Member Enum Member Description FaceAndNormalVector The interior specified by providing a face and a normal. Point The interior specified by providing a point. CavityPoints The interior specified by cavity points. FromExterior Wrap from the exterior. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-