FaceFromBoundaryBuilder Class¶
-
class
NXOpen.CAE.
FaceFromBoundaryBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Polygon Face by boundary
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreateFaceFromBoundaryBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
EdgeSelection | Returns the polygon edge selection to create a face from boundary |
FirstPtSelect | Returns or sets the first pt to join the ends of open edges in the loop. |
PolygonBodySelection | Returns the polygon body selection to assign the newly created face |
SecondPtSelect | Returns or sets the second pt to join the ends of open edges in the loop. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddSelectedPointPairs | Designate the join of the first and second pt by a straight edge (joining the ends of open loop segments). |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EdgeSelection¶
-
FaceFromBoundaryBuilder.
EdgeSelection
¶ Returns the polygon edge selection to create a face from boundary
-------------------------------------
Getter Method
Signature
EdgeSelection
Returns: Return type: NXOpen.CAE.SelectCAEEdgeList
New in version NX8.5.0.
License requirements: None.
FirstPtSelect¶
-
FaceFromBoundaryBuilder.
FirstPtSelect
¶ Returns or sets the first pt to join the ends of open edges in the loop.
-------------------------------------
Getter Method
Signature
FirstPtSelect
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstPtSelect
Parameters: firstPtSelect ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: None.
PolygonBodySelection¶
-
FaceFromBoundaryBuilder.
PolygonBodySelection
¶ Returns the polygon body selection to assign the newly created face
-------------------------------------
Getter Method
Signature
PolygonBodySelection
Returns: Return type: NXOpen.CAE.SelectCAEBody
New in version NX8.5.0.
License requirements: None.
SecondPtSelect¶
-
FaceFromBoundaryBuilder.
SecondPtSelect
¶ Returns or sets the second pt to join the ends of open edges in the loop.
-------------------------------------
Getter Method
Signature
SecondPtSelect
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondPtSelect
Parameters: secondPtSelect ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: None.
Method Detail¶
AddSelectedPointPairs¶
-
FaceFromBoundaryBuilder.
AddSelectedPointPairs
¶ Designate the join of the first and second pt by a straight edge (joining the ends of open loop segments).
Signature
AddSelectedPointPairs()
New in version NX8.5.0.
License requirements: None.
Validate¶
-
FaceFromBoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.