ArrayRecord2D Class |
Manages the 2d array record |
ArrayRecord2DEven Class |
Manages the 2d array record with even abscissa data |
ArrayRecord3D Class |
Manages the 3d array record |
BaseRecord Class |
Manages the base record. |
BaseUnit Class |
Manages the base unit |
ComplexSectionBasedMatrixRecord Class |
Represents a section based matrix record which has complex data values. |
DataManager Class |
Ftk data manager |
FTKManager Class |
FTK function data manager |
IApplicationData Class |
Represents the interface for application specific data class |
IApplicationDataOwner Class |
Represents the interface for application specific data owner |
Op2Record Class |
Represents the op2 record data |
OptionSetting Class |
Manager the options data for AFU Data Record |
RealSectionBasedMatrixRecord Class |
Represents a section based matrix record which has real data values. |
SectionBasedMatrixRecord Class |
Represents a kind of record data could be displayed by 3D graphing. |