DataManagerFileContainerType Enumeration¶
NXOpen.CAE.FTK.DataManager.FileContainerType is an alias for NXOpen.CAE.FTK.DataManagerFileContainerType
-
class
NXOpen.CAE.FTK.
DataManagerFileContainerType
¶ Bases:
object
Represents the file container type
Enum Members
Enum Member Enum Member Description NotSet Not any container AssociatedContainer Part associated container which has the same simple name with the part ResultContainer Solution result container which has the same name with the solution UserContainer User container All All containers -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-