FEModelOccAttributeAltRepMassUnitType Enumeration¶
NXOpen.CAE.FEModelOccAttribute.AltRepMassUnitType is an alias for NXOpen.CAE.FEModelOccAttributeAltRepMassUnitType
-
class
NXOpen.CAE.
FEModelOccAttributeAltRepMassUnitType
¶ Bases:
object
Represents the mass units types when in alt rep
Enum Members
Enum Member Enum Member Description G Mass unit of gram Kg Mass unit of kilogram Mg Mass unit of megagram T Mass unit of tonnes Lbm Mass unit of pound-mass Slug Mass unit of slug or (LBF-SEC^2)/FT Inchlbfsec2In Mass unit of (LBF-SEC^2)/IN Mmkgfsec2M Mass unit of (KGF-SEC^2)/M Kgfsec2Cm Mass unit of (KGF-SEC^2)/CM Kgfsec2Mm Mass unit of (KGF-SEC^2)/MM -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-