FEModelOccAttributeAltRepLengthUnitType Enumeration¶
NXOpen.CAE.FEModelOccAttribute.AltRepLengthUnitType is an alias for NXOpen.CAE.FEModelOccAttributeAltRepLengthUnitType
-
class
NXOpen.CAE.
FEModelOccAttributeAltRepLengthUnitType
¶ Bases:
object
Represents the length units types when in alt rep
Enum Members
Enum Member Enum Member Description Km Length unit of kilometer M Length unit of meter Cm Length unit of centimeter Mm Length unit of millimeter Micron Length unit of micrometer Nm Length unit of nanometer An Length unit of angstrom Mi Length unit of miles Ft Length unit of foot Inch Length unit of inch -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-