FEModelOccAttributeAltRepDisplayStyle Enumeration¶
NXOpen.CAE.FEModelOccAttribute.AltRepDisplayStyle is an alias for NXOpen.CAE.FEModelOccAttributeAltRepDisplayStyle
-
class
NXOpen.CAE.
FEModelOccAttributeAltRepDisplayStyle
¶ Bases:
object
Represents the display style when in alt rep
Enum Members
Enum Member Enum Member Description NotSet No graphics when in alt rep Approx Display approximation of base fem when in alt rep Symbol Display alternate rep symbol when when in alt rep Simplified Display simplified graphic defined by superelement file -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-