FEModelIdSpecificationObject_Struct Struct¶
NXOpen.CAE.FEModel.IdSpecificationObject is an alias for NXOpen.CAE.FEModelIdSpecificationObject_Struct
-
class
NXOpen.CAE.
FEModelIdSpecificationObject_Struct
¶ Bases:
object
Structure to specify the Node, Element, and Physical property table start ids and offsets for use in
CAE.FEModel.AppendFemodel()
.Constructor: NXOpen.CAE.FEModel.IdSpecificationObject()
Fields¶
Field | Description |
---|---|
FemObjectPrependName | String to prepend to fem object names such as element collector, material and section |
NodeStartId | Start id to use for imported nodes |
NodeIdOffset | If true node_start_id will be used as an offset for imported node ids |
ElementStartId | Start id to use for imported elements |
ElementIdOffset | If true element_start_id will be used as an offset for imported element ids |
PhysicalPropertyTableStartId | Start id to use for imported physical property tables |
PhysicalPropertyTableIdOffset | If true physical_property_table_start_id will be used as an offset for imported physical property table ids |
FemObjectPrependName¶
-
FEModelIdSpecificationObject_Struct.
FemObjectPrependName
¶ String to prepend to fem object names such as element collector, material and section
-------------------------------------
Field Value Type:str
NodeStartId¶
-
FEModelIdSpecificationObject_Struct.
NodeStartId
¶ Start id to use for imported nodes
-------------------------------------
Field Value Type:int
NodeIdOffset¶
-
FEModelIdSpecificationObject_Struct.
NodeIdOffset
¶ If true node_start_id will be used as an offset for imported node ids
-------------------------------------
Field Value Type:bool
ElementStartId¶
-
FEModelIdSpecificationObject_Struct.
ElementStartId
¶ Start id to use for imported elements
-------------------------------------
Field Value Type:int
ElementIdOffset¶
-
FEModelIdSpecificationObject_Struct.
ElementIdOffset
¶ If true element_start_id will be used as an offset for imported element ids
-------------------------------------
Field Value Type:bool