ElementTypesShape Enumeration¶
NXOpen.CAE.ElementTypes.Shape is an alias for NXOpen.CAE.ElementTypesShape
-
class
NXOpen.CAE.
ElementTypesShape
¶ Bases:
object
Specifies different CAE Element Shape types
Enum Members
Enum Member Enum Member Description Undefined Undefined Point Point Line Line Tri Triagular Quad Quadralateral Tet Tetrahedral Pyr Pyramid Wed Wedge Hex Hexagonal Spider Spider -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-