ElementTypeBuilderElementType Enumeration¶
NXOpen.CAE.ElementTypeBuilder.ElementType is an alias for NXOpen.CAE.ElementTypeBuilderElementType
-
class
NXOpen.CAE.
ElementTypeBuilderElementType
¶ Bases:
object
Dimension of the element types to be specified.
Enum Members
Enum Member Enum Member Description Point 0D element Beam beam Shell shell FreeSolid Free mesh solid SweepSolid Sweep mesh solid SweepSolidWedge Sweep mesh solid with wedges Spider Spider Connection Connection Connection AnySolid Any solid TriaShell Tria shell QuadShell Quad shell Weld Weld element Contact Contact element Pyramid Pyramid -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-