ElementTypeBuilderElementOrderType Enumeration¶
NXOpen.CAE.ElementTypeBuilder.ElementOrderType is an alias for NXOpen.CAE.ElementTypeBuilderElementOrderType
-
class
NXOpen.CAE.
ElementTypeBuilderElementOrderType
¶ Bases:
object
Order of the element types to be specified.
Enum Members
Enum Member Enum Member Description Any any element Linear linear element Parabolic parabolic element -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-