ElementTranslateBuilderCopyType Enumeration¶
NXOpen.CAE.ElementTranslateBuilder.CopyType is an alias for NXOpen.CAE.ElementTranslateBuilderCopyType
-
class
NXOpen.CAE.
ElementTranslateBuilderCopyType
¶ Bases:
object
the copy types
Enum Members
Enum Member Enum Member Description TranslateOnly translate without copying elements CopyTranslate first copy elements then translate the copies ElementCoat make 1D element using the existing nodes -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-