ElementSplitBuilderSplitMethodType Enumeration¶
NXOpen.CAE.ElementSplitBuilder.SplitMethodType is an alias for NXOpen.CAE.ElementSplitBuilderSplitMethodType
-
class
NXOpen.CAE.
ElementSplitBuilderSplitMethodType
¶ Bases:
object
the split method types
Enum Members
Enum Member Enum Member Description SeedElement by vector comparison ExistingConnectivity use existing element connectivity InteractiveMouseLocation Interactive Element Split ElementShape Based on element shape ShortestDiagonal Shortest Dialgonal -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-