ElementReflectBuilderNewMeshType Enumeration¶
NXOpen.CAE.ElementReflectBuilder.NewMeshType is an alias for NXOpen.CAE.ElementReflectBuilderNewMeshType
-
class
NXOpen.CAE.
ElementReflectBuilderNewMeshType
¶ Bases:
object
Option to create new mesh or add to existing mesh
Enum Members
Enum Member Enum Member Description Create create new mesh Existing add to existing mesh -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-