ElementModifyOrderBuilder Class¶
-
class
NXOpen.CAE.
ElementModifyOrderBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementModifyOrderBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementModifyOrderBuilder()
New in version NX6.0.1.
Properties¶
Property | Description |
---|---|
ElementType | Returns the element type to be created |
Jacobian | Returns the jacobian value to be used for creating mixed type midnodes |
MeshSelection | Returns the selected mesh(es) |
MidnodeType | Returns or sets the midnode option |
OperationType | Returns or sets the operation option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitMesh | Commites the mesh. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementModifyOrderBuilderMidnode Enumeration | Represents the options for midnodes |
ElementModifyOrderBuilderOperation Enumeration | Represents the options for type of operation |
Property Detail¶
ElementType¶
-
ElementModifyOrderBuilder.
ElementType
¶ Returns the element type to be created
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.1.
License requirements: None.
Jacobian¶
-
ElementModifyOrderBuilder.
Jacobian
¶ Returns the jacobian value to be used for creating mixed type midnodes
-------------------------------------
Getter Method
Signature
Jacobian
Returns: Return type: NXOpen.Expression
New in version NX6.0.1.
License requirements: None.
MeshSelection¶
-
ElementModifyOrderBuilder.
MeshSelection
¶ Returns the selected mesh(es)
-------------------------------------
Getter Method
Signature
MeshSelection
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX6.0.1.
License requirements: None.
MidnodeType¶
-
ElementModifyOrderBuilder.
MidnodeType
¶ Returns or sets the midnode option
-------------------------------------
Getter Method
Signature
MidnodeType
Returns: Return type: NXOpen.CAE.ElementModifyOrderBuilderMidnode
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MidnodeType
Parameters: midnodeType ( NXOpen.CAE.ElementModifyOrderBuilderMidnode
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
OperationType¶
-
ElementModifyOrderBuilder.
OperationType
¶ Returns or sets the operation option
-------------------------------------
Getter Method
Signature
OperationType
Returns: Return type: NXOpen.CAE.ElementModifyOrderBuilderOperation
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
OperationType
Parameters: operationType ( NXOpen.CAE.ElementModifyOrderBuilderOperation
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
CommitMesh¶
-
ElementModifyOrderBuilder.
CommitMesh
¶ Commites the mesh.
Signature
CommitMesh()
Returns: Return type: list of NXOpen.CAE.Mesh
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
ElementModifyOrderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.