ElementExtrudeBuilder Class¶
-
class
NXOpen.CAE.
ElementExtrudeBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementExtrudeBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementExtrudeBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Axis | Returns or sets the axis. |
CollectorName | Returns or sets the mesh collector name |
Distance | Returns the distance |
DistanceOption | Returns or sets the distance option |
Edge | Returns the edge when extrude along path |
ElementDimensionOption | Returns or sets the element dimension option |
ElementType | Returns the element type builder. |
Elements | Returns the selected elements |
ExportMesh | Returns or sets the option which indicates whether mesh is exported to solver or not. |
Face | Returns the face when extrude by project to surface |
FlipState | Returns or sets the flip state from the builder |
Increment | Returns or sets the increment |
Label | Returns or sets the label |
MeshName | Returns or sets the mesh name |
MethodOption | Returns or sets the method option |
NeutralName | Returns or sets the element neutral name |
NewMeshOption | Returns or sets the new mesh option |
NumberOfCopy | Returns or sets the number of copy |
PercentOffset | Returns or sets the percent offset |
RetainCollector | Returns or sets the the flag which decides whether collectors are to be retained or not |
Tag | Returns the Tag for this object. |
TwistAngle | Returns the twist angle |
TwistOrigin | Returns or sets the twist origin |
Vector | Returns or sets the vector when extrude along vector |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Flip | Flip the direction of extrude - not journalled |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementExtrudeBuilderDistanceType Enumeration | Distance option |
ElementExtrudeBuilderElemDimType Enumeration | Dimension of element to be created |
ElementExtrudeBuilderMethodType Enumeration | Extrusion method |
ElementExtrudeBuilderNewMeshType Enumeration | Option to create new mesh or add to existing mesh |
Property Detail¶
Axis¶
-
ElementExtrudeBuilder.
Axis
¶ Returns or sets the axis.
-------------------------------------
Getter Method
Signature
Axis
Returns: Return type: NXOpen.Axis
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis
Parameters: axis ( NXOpen.Axis
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CollectorName¶
-
ElementExtrudeBuilder.
CollectorName
¶ Returns or sets the mesh collector name
-------------------------------------
Getter Method
Signature
CollectorName
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollectorName
Parameters: collectorName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Distance¶
-
ElementExtrudeBuilder.
Distance
¶ Returns the distance
-------------------------------------
Getter Method
Signature
Distance
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
DistanceOption¶
-
ElementExtrudeBuilder.
DistanceOption
¶ Returns or sets the distance option
-------------------------------------
Getter Method
Signature
DistanceOption
Returns: Return type: NXOpen.CAE.ElementExtrudeBuilderDistanceType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceOption
Parameters: distanceOption ( NXOpen.CAE.ElementExtrudeBuilderDistanceType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Edge¶
-
ElementExtrudeBuilder.
Edge
¶ Returns the edge when extrude along path
-------------------------------------
Getter Method
Signature
Edge
Returns: Return type: NXOpen.CAE.SelectCAEEdge
New in version NX5.0.0.
License requirements: None.
ElementDimensionOption¶
-
ElementExtrudeBuilder.
ElementDimensionOption
¶ Returns or sets the element dimension option
-------------------------------------
Getter Method
Signature
ElementDimensionOption
Returns: Return type: NXOpen.CAE.ElementExtrudeBuilderElemDimType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElementDimensionOption
Parameters: elementDimensionOption ( NXOpen.CAE.ElementExtrudeBuilderElemDimType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementType¶
-
ElementExtrudeBuilder.
ElementType
¶ Returns the element type builder.
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
ElementExtrudeBuilder.
Elements
¶ Returns the selected elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX5.0.0.
License requirements: None.
ExportMesh¶
-
ElementExtrudeBuilder.
ExportMesh
¶ Returns or sets the option which indicates whether mesh is exported to solver or not.
-------------------------------------
Getter Method
Signature
ExportMesh
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExportMesh
Parameters: fExportMesh (bool) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Face¶
-
ElementExtrudeBuilder.
Face
¶ Returns the face when extrude by project to surface
-------------------------------------
Getter Method
Signature
Face
Returns: Return type: NXOpen.CAE.SelectCAEFaceList
New in version NX5.0.0.
License requirements: None.
FlipState¶
-
ElementExtrudeBuilder.
FlipState
¶ Returns or sets the flip state from the builder
-------------------------------------
Getter Method
Signature
FlipState
Returns: Return type: int New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
FlipState
Parameters: flipstate (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Increment¶
-
ElementExtrudeBuilder.
Increment
¶ Returns or sets the increment
-------------------------------------
Getter Method
Signature
Increment
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Increment
Parameters: increment (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Label¶
-
ElementExtrudeBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshName¶
-
ElementExtrudeBuilder.
MeshName
¶ Returns or sets the mesh name
-------------------------------------
Getter Method
Signature
MeshName
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshName
Parameters: meshName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MethodOption¶
-
ElementExtrudeBuilder.
MethodOption
¶ Returns or sets the method option
-------------------------------------
Getter Method
Signature
MethodOption
Returns: Return type: NXOpen.CAE.ElementExtrudeBuilderMethodType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodOption
Parameters: methodOption ( NXOpen.CAE.ElementExtrudeBuilderMethodType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NeutralName¶
-
ElementExtrudeBuilder.
NeutralName
¶ Returns or sets the element neutral name
-------------------------------------
Getter Method
Signature
NeutralName
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NeutralName
Parameters: neutralName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewMeshOption¶
-
ElementExtrudeBuilder.
NewMeshOption
¶ Returns or sets the new mesh option
-------------------------------------
Getter Method
Signature
NewMeshOption
Returns: Return type: NXOpen.CAE.ElementExtrudeBuilderNewMeshType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewMeshOption
Parameters: newMeshOption ( NXOpen.CAE.ElementExtrudeBuilderNewMeshType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumberOfCopy¶
-
ElementExtrudeBuilder.
NumberOfCopy
¶ Returns or sets the number of copy
-------------------------------------
Getter Method
Signature
NumberOfCopy
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfCopy
Parameters: numberOfCopy (int) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PercentOffset¶
-
ElementExtrudeBuilder.
PercentOffset
¶ Returns or sets the percent offset
-------------------------------------
Getter Method
Signature
PercentOffset
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PercentOffset
Parameters: percentOffset (float) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
RetainCollector¶
-
ElementExtrudeBuilder.
RetainCollector
¶ Returns or sets the the flag which decides whether collectors are to be retained or not
-------------------------------------
Getter Method
Signature
RetainCollector
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RetainCollector
Parameters: isRetain (bool) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TwistAngle¶
-
ElementExtrudeBuilder.
TwistAngle
¶ Returns the twist angle
-------------------------------------
Getter Method
Signature
TwistAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
TwistOrigin¶
-
ElementExtrudeBuilder.
TwistOrigin
¶ Returns or sets the twist origin
-------------------------------------
Getter Method
Signature
TwistOrigin
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwistOrigin
Parameters: twistOrigin ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Vector¶
-
ElementExtrudeBuilder.
Vector
¶ Returns or sets the vector when extrude along vector
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Flip¶
-
ElementExtrudeBuilder.
Flip
¶ Flip the direction of extrude - not journalled
Signature
Flip()
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
ElementExtrudeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.