ElementDetachBuilder Class¶
-
class
NXOpen.CAE.
ElementDetachBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementDetachBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementDetachBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DetachNodeOption | Returns or sets the option which indicates whether all detachment nodes are to be selected. |
DetachmentNodes | Returns the nodes which will take part in detachment |
ElementSelection | Returns the selected elements which are to be detached |
NewMeshOption | Returns or sets the option which indicates whether to create a new mesh out of detached elements. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DetachNodeOption¶
-
ElementDetachBuilder.
DetachNodeOption
¶ Returns or sets the option which indicates whether all detachment nodes are to be selected.
-------------------------------------
Getter Method
Signature
DetachNodeOption
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DetachNodeOption
Parameters: fDetachNode (bool) – New in version NX11.0.0.
License requirements: None.
DetachmentNodes¶
-
ElementDetachBuilder.
DetachmentNodes
¶ Returns the nodes which will take part in detachment
-------------------------------------
Getter Method
Signature
DetachmentNodes
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX11.0.0.
License requirements: None.
ElementSelection¶
-
ElementDetachBuilder.
ElementSelection
¶ Returns the selected elements which are to be detached
-------------------------------------
Getter Method
Signature
ElementSelection
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX11.0.0.
License requirements: None.
NewMeshOption¶
-
ElementDetachBuilder.
NewMeshOption
¶ Returns or sets the option which indicates whether to create a new mesh out of detached elements.
-------------------------------------
Getter Method
Signature
NewMeshOption
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewMeshOption
Parameters: fNewMesh (bool) – New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ElementDetachBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.