ElementCreateBuilderElemDimType Enumeration¶
NXOpen.CAE.ElementCreateBuilder.ElemDimType is an alias for NXOpen.CAE.ElementCreateBuilderElemDimType
-
class
NXOpen.CAE.
ElementCreateBuilderElemDimType
¶ Bases:
object
Dimension of the element to be created
Enum Members
Enum Member Enum Member Description Point 0D element Beam beam Shell shell Solid solid, types currently supported through UI AnySolid any solid type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-