ElementConnectivityBuilderTypes Enumeration

NXOpen.CAE.ElementConnectivityBuilder.Types is an alias for NXOpen.CAE.ElementConnectivityBuilderTypes

class NXOpen.CAE.ElementConnectivityBuilderTypes

Bases: object

Modify connectivity types

Enum Members

Enum Member Enum Member Description
SingleElement Modify connectivity of selected element.
AllElementsAttachedToNode Modify connectivities of all attached elements to nodes.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.