ElementConnectivityBuilderMethods Enumeration¶
NXOpen.CAE.ElementConnectivityBuilder.Methods is an alias for NXOpen.CAE.ElementConnectivityBuilderMethods
-
class
NXOpen.CAE.
ElementConnectivityBuilderMethods
¶ Bases:
object
Available modify connectivity methods
Enum Members
Enum Member Enum Member Description ReplaceNode Replace a node of an element by another one SwapEnds Swap the nodes of a 2-noded element ModifyLegs Add or delete leg nodes of spider element -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-