EdgeSticherBuilder Class¶
-
class
NXOpen.CAE.
EdgeSticherBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.EdgeSticherBuilder
To create a new instance of this class, use
NXOpen.CAE.FemPart.CreateEdgeSticherBuilder()
Default values.
Property Value SearchDistance.Value 0.1 (millimeters part), 0.004 (inches part) SnapEnds.Value 0.1 (millimeters part), 0.004 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BodySelection | Returns the body selection for Auto-Stitch Edge |
ExclusionEdgeSelection | Returns the edges to be excluded from auto-stitch operation |
SearchDistance | Returns the search distance value to check overlap |
SnapEnds | Returns the snap ends value to snap to vertex at the end of edge |
SourceEdgeSelection | Returns the source edge selection for Stitch Edge |
StitchMethod | Returns or sets the stitch method |
StitchOption | Returns or sets the operand type for auto-stitch edge |
Tag | Returns the Tag for this object. |
TargetEdgeSelection | Returns the target edge selection for stitch edge when type is NXOpen.CAE.EdgeSticherBuilderTypes.ManualEdgeToEdge |
TargetFaceSelection | Returns the target face selection for stitch edge when type is NXOpen.CAE.EdgeSticherBuilderTypes.ManualEdgeToFace |
Type | Returns or sets the type : (Obsolete from NX07. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EdgeSticherBuilderStitchMethods Enumeration | Stitch method : NX7. |
EdgeSticherBuilderStitchOptions Enumeration | Stitch option for stitch : NX7. |
EdgeSticherBuilderTypes Enumeration | Type of edge stitch : For Pre-NX7. |
Property Detail¶
BodySelection¶
-
EdgeSticherBuilder.
BodySelection
¶ Returns the body selection for Auto-Stitch Edge
-------------------------------------
Getter Method
Signature
BodySelection
Returns: Return type: NXOpen.CAE.SelectCAEBodyList
New in version NX7.0.0.
License requirements: None.
ExclusionEdgeSelection¶
-
EdgeSticherBuilder.
ExclusionEdgeSelection
¶ Returns the edges to be excluded from auto-stitch operation
-------------------------------------
Getter Method
Signature
ExclusionEdgeSelection
Returns: Return type: NXOpen.CAE.SelectCAEEdgeList
New in version NX7.0.0.
License requirements: None.
SearchDistance¶
-
EdgeSticherBuilder.
SearchDistance
¶ Returns the search distance value to check overlap
-------------------------------------
Getter Method
Signature
SearchDistance
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SnapEnds¶
-
EdgeSticherBuilder.
SnapEnds
¶ Returns the snap ends value to snap to vertex at the end of edge
-------------------------------------
Getter Method
Signature
SnapEnds
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SourceEdgeSelection¶
-
EdgeSticherBuilder.
SourceEdgeSelection
¶ Returns the source edge selection for Stitch Edge
-------------------------------------
Getter Method
Signature
SourceEdgeSelection
Returns: Return type: NXOpen.CAE.SelectCAEEdgeList
New in version NX6.0.0.
License requirements: None.
StitchMethod¶
-
EdgeSticherBuilder.
StitchMethod
¶ Returns or sets the stitch method
-------------------------------------
Getter Method
Signature
StitchMethod
Returns: Return type: NXOpen.CAE.EdgeSticherBuilderStitchMethods
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StitchMethod
Parameters: type ( NXOpen.CAE.EdgeSticherBuilderStitchMethods
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
StitchOption¶
-
EdgeSticherBuilder.
StitchOption
¶ Returns or sets the operand type for auto-stitch edge
-------------------------------------
Getter Method
Signature
StitchOption
Returns: Return type: NXOpen.CAE.EdgeSticherBuilderStitchOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StitchOption
Parameters: stitchOption ( NXOpen.CAE.EdgeSticherBuilderStitchOptions
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetEdgeSelection¶
-
EdgeSticherBuilder.
TargetEdgeSelection
¶ Returns the target edge selection for stitch edge when type is
NXOpen.CAE.EdgeSticherBuilderTypes.ManualEdgeToEdge
-------------------------------------
Getter Method
Signature
TargetEdgeSelection
Returns: Return type: NXOpen.CAE.SelectCAEEdgeList
New in version NX6.0.0.
License requirements: None.
TargetFaceSelection¶
-
EdgeSticherBuilder.
TargetFaceSelection
¶ Returns the target face selection for stitch edge when type is
NXOpen.CAE.EdgeSticherBuilderTypes.ManualEdgeToFace
-------------------------------------
Getter Method
Signature
TargetFaceSelection
Returns: Return type: NXOpen.CAE.SelectCAEFaceList
New in version NX6.0.0.
License requirements: None.
Type¶
-
EdgeSticherBuilder.
Type
¶ Returns or sets the type : (Obsolete from NX07.
5 onwards)
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.CAE.EdgeSticherBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.CAE.EdgeSticherBuilderTypes
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
EdgeSticherBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.