EdgePathMethod Class¶
-
class
NXOpen.CAE.
EdgePathMethod
¶ Bases:
NXOpen.SelectionMethod
Represents a
NXOpen.CAE.EdgePathMethod
.The edge path method is used by other objects to define a start point (
NXOpen.CAE.CAEVertex
) and a path defined by connected CAE edges (NXOpen.CAE.CAEEdge
). The path is defined by adding seed edges which are each defined by a start point (NXOpen.CAE.CAEVertex
) and a an edge (NXOpen.CAE.CAEEdge
). The path object uses these seeds as input to an algorithm which will determine the complete, coninuous, path. If the resultant path is not the one desired, this indicates that too few seeds were specified. The path class does not allow a curve to be used more than once in a path. CallingNXOpen.CAE.EdgePathMethod.FlipPath()
will flip the direction of the path definition, such that subsequent calls toNXOpen.CAE.EdgePathMethod.GetSeedEdges()
orNXOpen.CAE.EdgePathMethod.GetPathEdges()
will return seed or path edges in the new, flipped, order along with correspondingly updated start vertices.To obtain an instance of this class use CAE::SmartSelectionManager
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
AddSeedEdge | Add seed (start vertex and edge) to the end of the path. |
Dispose | Frees the object from memory. |
FlipPath | Flip the path start and end. |
GetPathEdges | Returns the resultant start vertics and edges of the path. |
GetSeedEdges | Returns the seed start vertices and edges which define the path. |
GetSeeds | Returns the seed start vertices and edges which define the path. |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
RemoveSeedEdge | Remove seed (start vertex and edge) from the path. |
Method Detail¶
AddSeedEdge¶
-
EdgePathMethod.
AddSeedEdge
¶ Overloaded method AddSeedEdge
AddSeedEdge(seedStartVertex, seedEdge)
AddSeedEdge(seedStartVertex, seedEdge, preferFreeEdges, allowGapJumping, gapJumpingTolerance)
-------------------------------------
Add seed (start vertex and edge) to the end of the path. The vertex defines the start point along the edge. If the addition of the seed would result in an invalid path, the seed will not be added and the function will return an error.
Signature
AddSeedEdge(seedStartVertex, seedEdge)
Parameters: - seedStartVertex (
NXOpen.CAE.CAEVertex
) – seed vertex - seedEdge (
NXOpen.CAE.CAEEdge
) – seed edge
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use overloaded
NXOpen.CAE.EdgePathMethod.AddSeedEdge()
with additional arguments instead.License requirements: None.
-------------------------------------
Add seed (start vertex and edge) to the end of the path. The vertex defines the start point along the edge. If the addition of the seed would result in an invalid path, the seed will not be added and the function will return an error.
Signature
AddSeedEdge(seedStartVertex, seedEdge, preferFreeEdges, allowGapJumping, gapJumpingTolerance)
Parameters: - seedStartVertex (
NXOpen.CAE.CAEVertex
) – seed vertex - seedEdge (
NXOpen.CAE.CAEEdge
) – seed edge - preferFreeEdges (bool) – if true, prefer free edges
- allowGapJumping (bool) – if true, gaps between edges will be jumped
- gapJumpingTolerance (float) –
New in version NX10.0.0.
License requirements: None.
-------------------------------------
FlipPath¶
-
EdgePathMethod.
FlipPath
¶ Flip the path start and end.
This changes the definition of the path such that subsequent calls to
NXOpen.CAE.EdgePathMethod.GetSeedEdges()
orNXOpen.CAE.EdgePathMethod.GetPathEdges()
will return seed or path edges in the new, flipped, order along with correspondingly updated start vertices.Signature
FlipPath()
New in version NX9.0.0.
License requirements: None.
GetPathEdges¶
-
EdgePathMethod.
GetPathEdges
¶ Returns the resultant start vertics and edges of the path.
These define a path which is continuous from start to end.
Signature
GetPathEdges()
Returns: a tuple Return type: A tuple consisting of (pathStartVertices, pathEdges). pathStartVertices is a list of NXOpen.CAE.CAEVertex
. resultant start vertices pathEdges is a list ofNXOpen.CAE.CAEEdge
. resultant edgesNew in version NX9.0.0.
License requirements: None.
GetSeedEdges¶
-
EdgePathMethod.
GetSeedEdges
¶ Returns the seed start vertices and edges which define the path.
The path object uses these seeds as input to an algorithm which will determine the complete, coninuous, path.
Signature
GetSeedEdges()
Returns: a tuple Return type: A tuple consisting of (seedStartVertices, seedEdges). seedStartVertices is a list of NXOpen.CAE.CAEVertex
. seed start vertices seedEdges is a list ofNXOpen.CAE.CAEEdge
. seed edgesNew in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.EdgePathMethod.GetSeeds()
instead.License requirements: None.
GetSeeds¶
-
EdgePathMethod.
GetSeeds
¶ Returns the seed start vertices and edges which define the path.
The path object uses these seeds as input to an algorithm which will determine the complete, coninuous, path. Each seed also specifies the options used by the path algorithm for that segment of the path.
Signature
GetSeeds()
Returns: a tuple Return type: A tuple consisting of (seedStartVertices, seedEdges, preferFreeEdges, allowGapJumping, gapJumpingTolerance). seedStartVertices is a list of NXOpen.CAE.CAEVertex
. seed start vertices seedEdges is a list ofNXOpen.CAE.CAEEdge
. seed edges preferFreeEdges is a list of bool. if true, prefer free edgesallowGapJumping is a list of bool. if true, gaps between edges will be jumpedgapJumpingTolerance is a list of float. if allowGapJumping is true, this is the tolerance to use for jumping gaps between edgesNew in version NX10.0.0.
License requirements: None.
RemoveSeedEdge¶
-
EdgePathMethod.
RemoveSeedEdge
¶ Remove seed (start vertex and edge) from the path.
If the removal of the seed would result in an invalid path, the seed will not be added and the function will return an error.
Signature
RemoveSeedEdge(seedEdge)
Parameters: seedEdge ( NXOpen.CAE.CAEEdge
) – seed edgeNew in version NX9.0.0.
License requirements: None.