EdgeFaceImprintBuilder Class¶
-
class
NXOpen.CAE.
EdgeFaceImprintBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Face Face Imprint
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreateEdgeFaceImprintBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
EdgeCurveSelection | Returns the edge/curve selection for projection imprint |
ExtendEdgeToBoundaryToggle | Returns or sets the stitch toggle state |
ProjectionDirectionMethod | Returns or sets the projection direction method |
ProjectionVector | Returns or sets the projection vector direction |
StitchToggle | Returns or sets the stitch toggle state |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face selection for projection imprint |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EdgeFaceImprintBuilderProjectionDirectionType Enumeration | the projection directon type |
Property Detail¶
EdgeCurveSelection¶
-
EdgeFaceImprintBuilder.
EdgeCurveSelection
¶ Returns the edge/curve selection for projection imprint
-------------------------------------
Getter Method
Signature
EdgeCurveSelection
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
ExtendEdgeToBoundaryToggle¶
-
EdgeFaceImprintBuilder.
ExtendEdgeToBoundaryToggle
¶ Returns or sets the stitch toggle state
-------------------------------------
Getter Method
Signature
ExtendEdgeToBoundaryToggle
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendEdgeToBoundaryToggle
Parameters: extendEdgetoBoundaryOpt (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ProjectionDirectionMethod¶
-
EdgeFaceImprintBuilder.
ProjectionDirectionMethod
¶ Returns or sets the projection direction method
-------------------------------------
Getter Method
Signature
ProjectionDirectionMethod
Returns: Return type: NXOpen.CAE.EdgeFaceImprintBuilderProjectionDirectionType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectionDirectionMethod
Parameters: projDirectionType ( NXOpen.CAE.EdgeFaceImprintBuilderProjectionDirectionType
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ProjectionVector¶
-
EdgeFaceImprintBuilder.
ProjectionVector
¶ Returns or sets the projection vector direction
-------------------------------------
Getter Method
Signature
ProjectionVector
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectionVector
Parameters: projectionVector ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
StitchToggle¶
-
EdgeFaceImprintBuilder.
StitchToggle
¶ Returns or sets the stitch toggle state
-------------------------------------
Getter Method
Signature
StitchToggle
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StitchToggle
Parameters: stitchOption (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TargetFace¶
-
EdgeFaceImprintBuilder.
TargetFace
¶ Returns the target face selection for projection imprint
-------------------------------------
Getter Method
Signature
TargetFace
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
EdgeFaceImprintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.