DurabilityStaticEventBuilderExcitationTypeEnum Enumeration¶
NXOpen.CAE.DurabilityStaticEventBuilder.ExcitationTypeEnum is an alias for NXOpen.CAE.DurabilityStaticEventBuilderExcitationTypeEnum
-
class
NXOpen.CAE.
DurabilityStaticEventBuilderExcitationTypeEnum
¶ Bases:
object
the static excitation type.
Enum Members
Enum Member Enum Member Description Pattern Pattern ResultPath Result Path Function Function -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-