DurabilitySolveOptionsCollection Class

class NXOpen.CAE.DurabilitySolveOptionsCollection

Bases: object

Represents a collection of correl meta solution.

To obtain an instance of this class, refer to NXOpen.CAE.DurabilityManager

New in version NX8.5.0.

Methods

Method Description
CloneSolveoptions Clones a durability event override.
CreateEventoverridesBuilder Creates the builder object of durability event overrides.
DeleteSolveoptions Delete a durability event overrides.
FindObject Finds an event override with a specified name.

Method Detail

CloneSolveoptions

DurabilitySolveOptionsCollection.CloneSolveoptions

Clones a durability event override.

Signature CloneSolveoptions(source)

Parameters:source (NXOpen.CAE.DurabilitySolveOptions) – Source event overrides
Returns:Cloned event overrides
Return type:NXOpen.CAE.DurabilitySolveOptions

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

CreateEventoverridesBuilder

DurabilitySolveOptionsCollection.CreateEventoverridesBuilder

Creates the builder object of durability event overrides.

Signature CreateEventoverridesBuilder(eventoverrides)

Parameters:eventoverrides (NXOpen.CAE.DurabilitySolveOptions) –
Returns:
Return type:NXOpen.CAE.DurabilityEventOverridesBuilder

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

DeleteSolveoptions

DurabilitySolveOptionsCollection.DeleteSolveoptions

Delete a durability event overrides.

Signature DeleteSolveoptions(eventoverrides)

Parameters:eventoverrides (NXOpen.CAE.DurabilitySolveOptions) – The durability event overrides to be deleted

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

FindObject

DurabilitySolveOptionsCollection.FindObject

Finds an event override with a specified name.

Signature FindObject(name)

Parameters:name (str) – name of the durability event override
Returns:The durability event override
Return type:NXOpen.CAE.DurabilitySolveOptions

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)