DurabilityResultPathBuilder Class¶
-
class
NXOpen.CAE.
DurabilityResultPathBuilder
¶ Bases:
NXOpen.CAE.DurabilityExcitationBuilder
Represents a
NXOpen.CAE.DurabilityResultPath
builder.There is no kf creator for this.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ExcitationName | Returns or sets the excitation name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddIteration | Adds an iteration. |
AddLoadcase | Adds a loadcase. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MoveLoadcaseDown | Moves a loadcase down by index. |
MoveLoadcaseUp | Moves a loadcase up by index. |
RemoveLoadcase | Removes a loadcase by index. |
SetScale | Sets the scale for a loadcase by index. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddIteration¶
-
DurabilityResultPathBuilder.
AddIteration
¶ Adds an iteration.
Signature
AddIteration(iteration)
Parameters: iteration (int) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
AddLoadcase¶
-
DurabilityResultPathBuilder.
AddLoadcase
¶ Adds a loadcase.
Signature
AddLoadcase(loadcase)
Parameters: loadcase (int) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MoveLoadcaseDown¶
-
DurabilityResultPathBuilder.
MoveLoadcaseDown
¶ Moves a loadcase down by index.
Signature
MoveLoadcaseDown(index)
Parameters: index (int) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MoveLoadcaseUp¶
-
DurabilityResultPathBuilder.
MoveLoadcaseUp
¶ Moves a loadcase up by index.
Signature
MoveLoadcaseUp(index)
Parameters: index (int) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
RemoveLoadcase¶
-
DurabilityResultPathBuilder.
RemoveLoadcase
¶ Removes a loadcase by index.
Signature
RemoveLoadcase(index)
Parameters: index (int) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
SetScale¶
-
DurabilityResultPathBuilder.
SetScale
¶ Sets the scale for a loadcase by index.
Signature
SetScale(index, scale)
Parameters: - index (int) –
- scale (float) –
New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Validate¶
-
DurabilityResultPathBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.