DurabilityRandomFatigueCollection Class

class NXOpen.CAE.DurabilityRandomFatigueCollection

Bases: object

Represents a collection of random fatigue.

To obtain an instance of this class, refer to NXOpen.CAE.DurabilityManager

New in version NX8.5.0.

Methods

Method Description
CloneRandomFatigue Clones a durability event fatigue settings.
CreateRandomfatigueBuilder Creates the builder object of durability event fatigue settings.
DeleteRandomFatigue Delete a durability fatigue.
FindObject Finds an event fatigue settings with a specified name.

Method Detail

CloneRandomFatigue

DurabilityRandomFatigueCollection.CloneRandomFatigue

Clones a durability event fatigue settings.

Signature CloneRandomFatigue(source)

Parameters:source (NXOpen.CAE.DurabilityRandomFatigue) – Source event fatigue settingss
Returns:Cloned random fatigue settingss
Return type:NXOpen.CAE.DurabilityRandomFatigue

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

CreateRandomfatigueBuilder

DurabilityRandomFatigueCollection.CreateRandomfatigueBuilder

Creates the builder object of durability event fatigue settings.

Signature CreateRandomfatigueBuilder(randomFatigue)

Parameters:randomFatigue (NXOpen.CAE.DurabilityRandomFatigue) –
Returns:
Return type:NXOpen.CAE.DurabilityRandomFatigueBuilder

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

DeleteRandomFatigue

DurabilityRandomFatigueCollection.DeleteRandomFatigue

Delete a durability fatigue.

Signature DeleteRandomFatigue(randomFatigue)

Parameters:randomFatigue (NXOpen.CAE.DurabilityRandomFatigue) – The durability random fatigue settings to be deleted

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

FindObject

DurabilityRandomFatigueCollection.FindObject

Finds an event fatigue settings with a specified name.

Signature FindObject(name)

Parameters:name (str) – name of the durability event fatigue settings
Returns:The durability random fatigue settings
Return type:NXOpen.CAE.DurabilityRandomFatigue

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)