DurabilityFatigueCollection Class

class NXOpen.CAE.DurabilityFatigueCollection

Bases: object

Represents a collection of event fatigue settings.

To obtain an instance of this class, refer to NXOpen.CAE.DurabilityManager

New in version NX8.5.0.

Methods

Method Description
CloneFatigue Clones a durability event fatigue settings.
CreateEventfatiguesettingsBuilder Creates the builder object of durability event fatigue settings.
DeleteFatigue Delete a durability fatigue.
FindObject Finds an event fatigue settings with a specified name.

Method Detail

CloneFatigue

DurabilityFatigueCollection.CloneFatigue

Clones a durability event fatigue settings.

Signature CloneFatigue(source)

Parameters:source (NXOpen.CAE.DurabilityFatigue) – Source event fatigue settingss
Returns:Cloned event fatigue settingss
Return type:NXOpen.CAE.DurabilityFatigue

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

CreateEventfatiguesettingsBuilder

DurabilityFatigueCollection.CreateEventfatiguesettingsBuilder

Creates the builder object of durability event fatigue settings.

Signature CreateEventfatiguesettingsBuilder(eventfatiguesettings)

Parameters:eventfatiguesettings (NXOpen.CAE.DurabilityFatigue) –
Returns:
Return type:NXOpen.CAE.DurabilityEventFatigueSettingsBuilder

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

DeleteFatigue

DurabilityFatigueCollection.DeleteFatigue

Delete a durability fatigue.

Signature DeleteFatigue(eventfatiguesettings)

Parameters:eventfatiguesettings (NXOpen.CAE.DurabilityFatigue) – The durability event fatigue settings to be deleted

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

FindObject

DurabilityFatigueCollection.FindObject

Finds an event fatigue settings with a specified name.

Signature FindObject(name)

Parameters:name (str) – name of the durability event fatigue settings
Returns:The durability event fatigue settings
Return type:NXOpen.CAE.DurabilityFatigue

New in version NX8.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)