DurabilityDataControlBuilder Class¶
-
class
NXOpen.CAE.
DurabilityDataControlBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a builder class for the transient event data control.
The data control helps choose the start and ending time for the transient loading. It also allows for a decimation order and a peak valley tolerance control. .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
DecimationOrder | Returns or sets the decimation order. |
OutputEndTime | Returns the output end time. |
OutputStartTime | Returns the output start time. |
PeakValleyTolerance | Returns or sets the peak valley tolerance. |
Tag | Returns the Tag for this object. |
TimeExtents | Returns or sets the time extents. |
Methods¶
Enumerations¶
DurabilityDataControlBuilderTimeExtentsEnum Enumeration | the time extents enum. |
Property Detail¶
DecimationOrder¶
-
DurabilityDataControlBuilder.
DecimationOrder
¶ Returns or sets the decimation order.
-------------------------------------
Getter Method
Signature
DecimationOrder
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DecimationOrder
Parameters: decimationOrder (int) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
OutputEndTime¶
-
DurabilityDataControlBuilder.
OutputEndTime
¶ Returns the output end time.
-------------------------------------
Getter Method
Signature
OutputEndTime
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
OutputStartTime¶
-
DurabilityDataControlBuilder.
OutputStartTime
¶ Returns the output start time.
-------------------------------------
Getter Method
Signature
OutputStartTime
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
PeakValleyTolerance¶
-
DurabilityDataControlBuilder.
PeakValleyTolerance
¶ Returns or sets the peak valley tolerance.
-------------------------------------
Getter Method
Signature
PeakValleyTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PeakValleyTolerance
Parameters: peakValleyTolerance (float) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
TimeExtents¶
-
DurabilityDataControlBuilder.
TimeExtents
¶ Returns or sets the time extents.
-------------------------------------
Getter Method
Signature
TimeExtents
Returns: Return type: NXOpen.CAE.DurabilityDataControlBuilderTimeExtentsEnum
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TimeExtents
Parameters: timeExtents ( NXOpen.CAE.DurabilityDataControlBuilderTimeExtentsEnum
) –New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)