DisplayNodalCsysBuilder Class¶
-
class
NXOpen.CAE.
DisplayNodalCsysBuilder
¶ Bases:
NXOpen.Builder
Represents a
CAE.DisplayNodalCsysBuilder
.To create a new instance of this class, use
NXOpen.CAE.NodeElementInfoManager.CreateDisplayNodalCsysBuilder()
Default values.
Property Value CsysTypeEnum Displacement SelectionTypeEnum EntireModel New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CsysTypeEnum | Returns or sets the coordinate system type |
NodeSelector | Returns the selection of nodes to display coordinate systems |
SelectionTypeEnum | Returns or sets the way selections will be displayed |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetColorXAxis | Returns the color for direction one |
GetColorYAxis | Returns the color for direction two |
GetColorZAxis | Returns the color for direction three |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetColorXAxis | Sets the color for direction one |
SetColorYAxis | Sets the color for direction two |
SetColorZAxis | Sets the color for direction three |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DisplayNodalCsysBuilderDisplayNodalCsysType Enumeration | the options to specify the type of coordinate system to display |
DisplayNodalCsysBuilderNodesToDisplayType Enumeration | the options to specify the scope of nodes to select |
Property Detail¶
CsysTypeEnum¶
-
DisplayNodalCsysBuilder.
CsysTypeEnum
¶ Returns or sets the coordinate system type
-------------------------------------
Getter Method
Signature
CsysTypeEnum
Returns: Return type: NXOpen.CAE.DisplayNodalCsysBuilderDisplayNodalCsysType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysTypeEnum
Parameters: csysTypeEnum ( NXOpen.CAE.DisplayNodalCsysBuilderDisplayNodalCsysType
) –New in version NX12.0.0.
License requirements: None.
NodeSelector¶
-
DisplayNodalCsysBuilder.
NodeSelector
¶ Returns the selection of nodes to display coordinate systems
-------------------------------------
Getter Method
Signature
NodeSelector
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX12.0.0.
License requirements: None.
SelectionTypeEnum¶
-
DisplayNodalCsysBuilder.
SelectionTypeEnum
¶ Returns or sets the way selections will be displayed
-------------------------------------
Getter Method
Signature
SelectionTypeEnum
Returns: Return type: NXOpen.CAE.DisplayNodalCsysBuilderNodesToDisplayType
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionTypeEnum
Parameters: selectionTypeEnum ( NXOpen.CAE.DisplayNodalCsysBuilderNodesToDisplayType
) –New in version NX12.0.0.
License requirements: None.
Method Detail¶
GetColorXAxis¶
GetColorYAxis¶
GetColorZAxis¶
SetColorXAxis¶
SetColorYAxis¶
SetColorZAxis¶
Validate¶
-
DisplayNodalCsysBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.