DependentMeshBuilderMeshType Enumeration¶
NXOpen.CAE.DependentMeshBuilder.MeshType is an alias for NXOpen.CAE.DependentMeshBuilderMeshType
-
class
NXOpen.CAE.
DependentMeshBuilderMeshType
¶ Bases:
object
The mesh type for face dependency
Enum Members
Enum Member Enum Member Description Free Free mesh Map Map mesh -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-