DataProcessingCollection Class¶
-
class
NXOpen.CAE.
DataProcessingCollection
¶ Bases:
object
Represents a collection of Data Processing meta solution.
To obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates a data processing object. |
CreateBuilder | Creates the builder object of DPM meta solution. |
DeleteDataProcessing | Deletes the DPM meta solution. |
FindObject | Finds an dpm meta solution with a specified name. |
Method Detail¶
Create¶
-
DataProcessingCollection.
Create
¶ Creates a data processing object.
Signature
Create(dataSource)
Parameters: dataSource ( NXOpen.CAE.DataSource
) – the data sourceReturns: Return type: NXOpen.CAE.DataProcessing
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateBuilder¶
-
DataProcessingCollection.
CreateBuilder
¶ Creates the builder object of DPM meta solution.
Signature
CreateBuilder(metasolution)
Parameters: metasolution ( NXOpen.CAE.DataProcessing
) –Returns: Return type: NXOpen.CAE.DataProcessingBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteDataProcessing¶
-
DataProcessingCollection.
DeleteDataProcessing
¶ Deletes the DPM meta solution.
Signature
DeleteDataProcessing(metasolution)
Parameters: metasolution ( NXOpen.CAE.DataProcessing
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
DataProcessingCollection.
FindObject
¶ Finds an dpm meta solution with a specified name.
Signature
FindObject(name)
Parameters: name (str) – name of the adpativity metasolution Returns: The DPM meta solution Return type: NXOpen.CAE.DataProcessing
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)