CorrelModePairingBuilderAuto Enumeration¶
NXOpen.CAE.CorrelModePairingBuilder.Auto is an alias for NXOpen.CAE.CorrelModePairingBuilderAuto
-
class
NXOpen.CAE.
CorrelModePairingBuilderAuto
¶ Bases:
object
The automatic pairing rule type
Enum Members
Enum Member Enum Member Description NotSet not automatic Sequential by mode numbers Frequency by frequency Mac by mac metric FreqMac by frequency AND mac -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-