CorrelFineTuneAlignmentBuilderAngleVector Enumeration

NXOpen.CAE.CorrelFineTuneAlignmentBuilder.AngleVector is an alias for NXOpen.CAE.CorrelFineTuneAlignmentBuilderAngleVector

class NXOpen.CAE.CorrelFineTuneAlignmentBuilderAngleVector

Bases: object

the angle vector enumeration for the alignment nudge

Enum Members

Enum Member Enum Member Description
Xc
Yc
Zc
NegXc
NegYc
NegZc
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.