ConvertToConvergentBodyBuilderOption Enumeration¶
NXOpen.CAE.ConvertToConvergentBodyBuilder.Option is an alias for NXOpen.CAE.ConvertToConvergentBodyBuilderOption
-
class
NXOpen.CAE.
ConvertToConvergentBodyBuilderOption
¶ Bases:
object
Represents the supported export locations of convergent body
Enum Members
Enum Member Enum Member Description ParentOfFEM The immediate parent of the current FEM Part ComponentOfCADBody The orginal component inside of assembly that polygon body is derived from in FEM Part NewPart The new part where the convergent body in the FEM part will be exported to ExistingPart The existing part where the convergent body in the FEM part will be exported to -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-