ContactMeshBuilderAlignmentType Enumeration

NXOpen.CAE.ContactMeshBuilder.AlignmentType is an alias for NXOpen.CAE.ContactMeshBuilderAlignmentType

class NXOpen.CAE.ContactMeshBuilderAlignmentType

Bases: object

the type of alignment to be created

Enum Members

Enum Member Enum Member Description
Minimumdistance
Normaltocontactedge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.