Adhesive Class |
Adhesive connection. |
Bolt Class |
Bolt connection. |
Bushing Class |
Bushing connection. |
ComponentData Class |
Composer connection. |
Composer Class |
Composer. |
ComposerData Class |
Composer connection. |
ConnectionDBData Class |
Connection DB data. |
ConnectionDBItemData Class |
Connection DB item data. |
ConnectionData Class |
Composer connection. |
CoordinatesLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
CoordinatesSeriesLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
CurveLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
Damper Class |
Damper connection. |
Element Class |
This is the class to access a connection element
|
ElementCollection Class |
Element collection provides methods to manage CAE.Connections.Element objects
|
FeEdgesLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
Folder Class |
The Folder class offers a way to create a hierarchy of connections and sub-folders
|
IConnection Class |
This class represents an interface to a connection object.
|
ICsys Class |
This class represents an Interface to the Connection Csys.
|
IDiameter Class |
This class represents an Interface to the Diameter parameters.
|
IDof Class |
This class represents an interface to the connection’s degrees of freedom.
|
IDofCombination Class |
This class represents an interface to the connection’s degrees of freedom combination.
|
IFlangesContainer Class |
This interface offers access to the flanges of a connection (SpotWeld for example). The flanges are used for specifying the connecting surfaces of the connection. Each flange can have one or more entities like meshes, elements etc.
|
IHeight Class |
This class represents an Interface to the Height parameters.
|
ILineDiscretization Class |
This class represents an Interface to the Diameter parameters.
|
ILineOffset Class |
This class represents an Interface to the Diameter parameters.
|
ILocationsContainer Class |
This class represents an Interface to the Locations parameters.
|
ILocationsMultiPointContainer Class |
This class represents an Interface to the Multi Point Locations container.
|
ILocationsSinglePointContainer Class |
This class represents an Interface to the Locations parameters.
|
ILocationsWithDirContainer Class |
This class represents an Interface to the Locations parameters.
|
ILocationsWithDiscretizationContainer Class |
This class represents an Interface to the Locations With Discretization container.
|
IMaterial Class |
This class represents an Interface to the Material entity.
|
INodalTargetCenter Class |
This class represents an Interface to the Connection Target.
|
INodalTargetLegs Class |
This class represents an Interface to the Connection Target.
|
INodalTargetsContainer Class |
This class represents an Interface to the Connection Target Container.
|
INodalTargetsPairing Class |
This class represents an Interface to the nodal connections pairing algorithm parameters.
|
IStiffness Class |
This class represents an Interface to the Stiffness constants.
|
IStiffnessDynamic Class |
This class represents an Interface to the Stiffness dynamic.
|
IStructuralDamping Class |
This class represents an Interface to the StructuralDamping constants.
|
IStructuralDampingDynamic Class |
This class represents an Interface to the StructuralDamping dynamic.
|
ITolerance Class |
This class represents an Interface to the Tolerance parameters.
|
IViscousDamping Class |
This class represents an Interface to the ViscousDamping constants.
|
IViscousDampingDynamic Class |
This class represents an Interface to the ViscousDamping dynamic.
|
IWidth Class |
This class represents an Interface to the Width parameters.
|
Kinematic Class |
Kinematic connection. |
Location Class |
Location base class. This defines connection locations with common properties like coordinates.
|
LocationWithDir Class |
Location With Direction interface. This defines connection locations with direction.
|
NodalTarget Class |
This class represents an Interface to the Connection Target.
|
NodalTargetSetOfPoints Class |
Set of Points Target. Use this interface to set/get parameters of the Set of Points Target type.
|
NodalTargetSinglePoint Class |
Group of Points Target. Use this interface to set/get parameters of the Group of Points Target type.
|
NodalTargetSpider Class |
Group of Points Target. Use this interface to set/get parameters of the Group of Points Target type.
|
NodeLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
NodeSeriesLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
PointLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
PointSeriesLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
Rigid Class |
Rigid connection. |
Sealing Class |
Sealing connection. |
SeamWeld Class |
Seam Weld connection. |
SelectionRecipeLocation Class |
Location interface. This defines connection locations with common properties like coordinates.
|
SpotWeld Class |
Spot Weld connection. |
Spring Class |
Spring connection. |
Utils Class |
Contains universal connections utility methods |