PointSeriesLocation Class¶
-
class
NXOpen.CAE.Connections.
PointSeriesLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
AddPoints | Add location nodes. |
GetPoints | Retrieve location points. |
GetXyzCoordinates | Gets the coordinates from the specified location. |
SetPoints | Set location points. |
Method Detail¶
AddPoints¶
-
PointSeriesLocation.
AddPoints
¶ Add location nodes.
Signature
AddPoints(points)
Parameters: points (list of NXOpen.Point
) – Points used for locationNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetPoints¶
-
PointSeriesLocation.
GetPoints
¶ Retrieve location points.
Signature
GetPoints()
Returns: Points used for location Return type: list of NXOpen.Point
New in version NX12.0.0.
License requirements: None.
SetPoints¶
-
PointSeriesLocation.
SetPoints
¶ Set location points.
Signature
SetPoints(points)
Parameters: points (list of NXOpen.Point
) – Points used for locationNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)