NodeSeriesLocation Class¶
-
class
NXOpen.CAE.Connections.
NodeSeriesLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
AddNodes | Add location nodes. |
GetNodes | Retrieve location nodes. |
GetXyzCoordinates | Gets the coordinates from the specified location. |
SetNodes | Set location nodes. |
Method Detail¶
AddNodes¶
-
NodeSeriesLocation.
AddNodes
¶ Add location nodes.
Signature
AddNodes(nodes)
Parameters: nodes (list of NXOpen.CAE.FENode
) – Node used for locationNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetNodes¶
-
NodeSeriesLocation.
GetNodes
¶ Retrieve location nodes.
Signature
GetNodes()
Returns: Node used for location Return type: list of NXOpen.CAE.FENode
New in version NX12.0.0.
License requirements: None.
SetNodes¶
-
NodeSeriesLocation.
SetNodes
¶ Set location nodes.
Signature
SetNodes(nodes)
Parameters: nodes (list of NXOpen.CAE.FENode
) – Node used for locationNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)