NodeLocation Class¶
-
class
NXOpen.CAE.Connections.
NodeLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Node | Returns or sets the FEM node used for creating the location. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetXyzCoordinates | Gets the coordinates from the specified location. |
Property Detail¶
Node¶
-
NodeLocation.
Node
¶ Returns or sets the FEM node used for creating the location.
If the location type is not node, this method will raise an error.
-------------------------------------
Getter Method
Signature
Node
Returns: Node used for location Return type: NXOpen.CAE.FENode
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Node
Parameters: node ( NXOpen.CAE.FENode
) – Node used for locationNew in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)