ModelizationResultType Enumeration¶
-
class
NXOpen.CAE.Connections.
ModelizationResultType
¶ Bases:
object
Modelization result type Enum Members
Enum Member Enum Member Description NotSet None Material Material Weights Interpolation element weights Section Section Csys Csys Stiffness Stiffness ViscousDamping ViscousDamping StructuralDamping StructuralDamping Dofs Dofs DynamicStiffness Dynamic Stiffness DynamicViscousDamping Dynamic ViscousDamping DynamicStructuralDamping Dynamic StructuralDamping -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-