LocationWithDir Class¶
-
class
NXOpen.CAE.Connections.
LocationWithDir
¶ Bases:
NXOpen.CAE.Connections.Location
Location With Direction interface. This defines connection locations with direction.
To obtain an instance of this object use the AddLocationWithDirection creators on the Connections
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
DirectionPoint | Returns or sets the point of the direction definition end point. |
DirectionType | Returns the direction type |
DirectionValue | Returns the direction value |
DirectionVector | Returns or sets the direction definition vector |
Point | Returns or sets the point of the direction definition start point. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetXyzCoordinates | Gets the coordinates from the specified location. |
Property Detail¶
DirectionPoint¶
-
LocationWithDir.
DirectionPoint
¶ Returns or sets the point of the direction definition end point.
-------------------------------------
Getter Method
Signature
DirectionPoint
Returns: Return type: NXOpen.Point
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
DirectionPoint
Parameters: direction ( NXOpen.Point
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DirectionType¶
-
LocationWithDir.
DirectionType
¶ Returns the direction type
-------------------------------------
Getter Method
Signature
DirectionType
Returns: Direction type Return type: NXOpen.CAE.Connections.LocationDirectionType
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DirectionValue¶
-
LocationWithDir.
DirectionValue
¶ Returns the direction value
-------------------------------------
Getter Method
Signature
DirectionValue
Returns: Return type: NXOpen.Vector3d
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DirectionVector¶
-
LocationWithDir.
DirectionVector
¶ Returns or sets the direction definition vector
-------------------------------------
Getter Method
Signature
DirectionVector
Returns: Return type: NXOpen.Direction
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
DirectionVector
Parameters: direction ( NXOpen.Direction
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Point¶
-
LocationWithDir.
Point
¶ Returns or sets the point of the direction definition start point.
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)