HeightType Enumeration¶
-
class
NXOpen.CAE.Connections.
HeightType
¶ Bases:
object
Types of height definitions Enum Members
Enum Member Enum Member Description Undefined Undefined height type, used for connections that don’t use this parameter User User defined thickness MeanOfFlangesThickness Mean of flanges thickness DistanceBetweenFlanges Distance between flanges DistanceBetweenFlangesMeanOfFlangesThickness Distance between flanges - Mean of flanges thickness DistanceBetweenFlangesMaxOfFlangesThickness Distance between flanges - Max of flanges thickness -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-