ElementType Enumeration¶
-
class
NXOpen.CAE.Connections.
ElementType
¶ Bases:
object
Element type Enum Members
Enum Member Enum Member Description NotSet None EHex8 Hex8 EHex8Spider Hex8 + Spider E1d 1D E1DSpider 1D + Spider ESpider Spider EBushing Bushing Elm ESpring Spring Elm EDamper Damper Elm ERigid Rigid Elm EKinematic Kinematic Elm ERigidConnector Rigid Connector ERigidRigidConnector Rigid Connector - Rigid Connector EInterpolationSpider Interpolation + Spider -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-