DofCombination Enumeration¶
-
class
NXOpen.CAE.Connections.
DofCombination
¶ Bases:
object
Degrees Of Freedom Combination types Enum Members
Enum Member Enum Member Description UserDefined User defined combination for all DOFs Clamp DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 fixed, DOF5 fixed, DOF6 fixed Spheric DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 free, DOF6 free Point DOF1 fixed, DOF2 free, DOF3 free, DOF4 free, DOF5 free, DOF6 free Slider DOF1 free, DOF2 fixed, DOF3 fixed, DOF4 fixed, DOF5 fixed, DOF6 fixed Pivot DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 fixed, DOF6 fixed SliderPivot DOF1 free, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 fixed, DOF6 fixed Cardan DOF1 fixed, DOF2 fixed, DOF3 fixed, DOF4 free, DOF5 fixed, DOF6 free -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-