CurveLocation Class¶
-
class
NXOpen.CAE.Connections.
CurveLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Curve | Returns or sets the CURVE used for creating the location. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetXyzCoordinates | Gets the coordinates from the specified location. |
Property Detail¶
Curve¶
-
CurveLocation.
Curve
¶ Returns or sets the CURVE used for creating the location.
If the location type is not curve, this method will raise an error.
-------------------------------------
Getter Method
Signature
Curve
Returns: Curve used for location Return type: NXOpen.IBaseCurve
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Curve
Parameters: curve ( NXOpen.IBaseCurve
) – Curve used for locationNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)