CoordinatesLocation Class¶
-
class
NXOpen.CAE.Connections.
CoordinatesLocation
¶ Bases:
NXOpen.CAE.Connections.Location
Location interface. This defines connection locations with common properties like coordinates.
To obtain an instance of this object use the AddLocation creators on the Connections
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
GetCoordinates | Gets the coordinates from the specified location. |
GetXyzCoordinates | Gets the coordinates from the specified location. |
SetCoordinates | Set the coordinates. |
Method Detail¶
GetCoordinates¶
-
CoordinatesLocation.
GetCoordinates
¶ Gets the coordinates from the specified location.
The location can be any type: coordinates, node or point. Its coordinates will be returned.
Signature
GetCoordinates()
Returns: Location coordinates Return type: NXOpen.Point3d
New in version NX11.0.0.
License requirements: None.
SetCoordinates¶
-
CoordinatesLocation.
SetCoordinates
¶ Set the coordinates.
Only for coordinates type location
Signature
SetCoordinates(coordinates)
Parameters: coordinates ( NXOpen.Point3d
) – The location coordinatesNew in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)