CompanionResult Class¶
-
class
NXOpen.CAE.
CompanionResult
¶ Bases:
NXOpen.TaggedObject
Represents additional results data that will augment a primary set of Analysis results associated to a
NXOpen.CAE.SimSolution
.Companion results do not have to have any FE Model data ( Nodes/Elements). Companion results will use FE Model data from primary results assosicated with the solution. To create/edit a CompanionResult you can use the
NXOpen.CAE.CompanionResultBuilder
Object.To create or edit an instance of this class, use
NXOpen.CAE.CompanionResultBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the name given to this Solutions Companion Result object. |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
Name¶
-
CompanionResult.
Name
¶ Returns or sets the name given to this Solutions Companion Result object.
Used for user display and identification purposes.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)